Skip to content

Community Projects

Over the years, Siemens has been steadily increasing collaboration with open source projects.

Below is a list of some of the major community projects we have been involved in.

Linux & Embedded

Civil Infrastructure Platform (CIP)

The CIP project is focused on providing an open source "base layer" of industrial grade software, including the super long-term supported CIP kernel. We co-founded this project in 2016, are now benefiting greatly from this community effort and are driving significant contributions.

cip-project


coreboot

Providing a fast, open, and secure solution for firmware, coreboot is perfectly suited to be part of our open source stacks. We have been contributing drivers as well as core functionality in coreboot.

coreboot


isar

Designed to combine the knowledge from building in Debian and Yocto, isar enables repeatable generation of Debian-based root filesystems with customizations. It is sponsored by and widely used at Siemens for creating reusable layers.

ilbers/isar


SWUpdate

SWUpdate has become the de-facto open source industry standard for software updates in embedded devices - including at Siemens. As such, we are also heavily involved and contribute to the upstream project.

sbabic/swupdate


u-boot

U-boot powers a variety of Siemens Embedded devices and we contribute regularly upstream. A growing number of Siemens boards are available in the U-boot source tree.

source.denx.de/u-boot/u-boot


xenomai

Xenomai provides resource-efficient real-time support for applications integrated into the Linux environment. Since we've been using it in multiple products, Siemens has been a key contributor for many years.

www.xenomai.org

gitlab.com/Xenomai/xenomai3/xenomai

Edge Ecosystems

Margo

The Margo initiative defines mechanisms for interoperable orchestration at scale of edge applications/workloads and devices. It will deliver the interoperability promise through an open standard, a reference implementation and comprehensive compliance testing toolkit. Margo unlocks barriers to innovation in complex multi-vendor environments and accelerates digital transformation for organizations of all sizes.

margo


SBOM

CycloneDX

CycloneDX is the international standard for Bills of Materials (ECMA-424) that we use for SBOMs at Siemens (via the 'Standard BOM' inner source project). The OWASP Foundation and the ECMA International Technical Committee for Software & System Transparency (TC54) drive the continued advancement of the specification.

cyclonedx/specification
cyclonedx/cyclonedx-core-java
cyclonedx/cyclonedx-python-lib

LicenseLynx

LicenseLynx maps license references found in the wild to canonical license identifiers.

licenselynx


License & Compliance

fossology

Fossology runs license, copyright and export control scans on your project, providing a clear picture using standard SPDX exports and human-readable files for distribution. It has helped automate our development efforts, and we have been involved in its development and maintenance for years.

fossology/fossology

Additional tools and libraries for FOSSology available as OSS:


sw360

Managing licensing for large numbers of software components can be tedious, and SW360 aims to automate and provide an overview for licensing workflows. It acts as a central hub providing a UI portal and as an API, and integrates with Fossology and other compliance tooling. Developed at Siemens and Bosch, it is now under the stewardship of the Eclipse Foundation.

eclipse/sw360

Additional tools and libraries for SW360 available as OSS:

DevOps

GitLab

Siemens has been contributing to GitLab for years, and our contributions have garnered GitLab MVP awards in 17.0, 16.1, 14.7, 14.5, 13.10, 13.4, 12.8, 12.7, 12.6, 10.8, 9.5, and 8.16. If our users report issues, we don't wait for tickets - we fix them upstream.

Some of our contributions you might have enjoyed if you use GitLab include x509-signed commits, test coverage visualization, admin mode, exploring and managing project topics, following users, along with many more features and bugfixes!

Read more on our DevOps journey at GitLab.

gitlab-org


python-gitlab

We try to automate as much of our infrastructure as possible, and keeping healthy libraries that power Infrastructure as Code is an essential part of this. Since 2018, Siemens has been helping maintain the python-gitlab library along with our friends in the community.

python-gitlab/python-gitlab


renovate

Keeping our software up-to-date and secure is among our highest priorities, and we've worked to incorporate seamless dependency updates in our workflows. We continue contributing features to renovate so that more and more technologies and languages we use can benefit from continuous updates.

Running a large GitLab instance, we've also focused on renovate's bot workflow itself. This led us to discover a security risk and to collaborate with renovate, along with GitLab, to provide its GitLab Bot security guidelines.

renovatebot/renovate


Web of Things

Web of Things describes a set of standards by the World Wide Web Consortium (W3C) for the interoperability of different Internet of Things (IoT) platforms and application domains. WoT standards have been created by Siemens and other W3C members to counter further fragmentation in the IoT. In this context, several tools and implementations have been developed to support the adoption of this new set of standards.

Siemens also supports the development of other open-source Web of Things projects such as WebThings (previously known as Mozilla WebThings), node-opcua and more.

Eclipse ediTDor

A tool for simply designing WoT Thing Descriptions and Thing Models.

eclipse/editdor


Eclipse Thingweb

Eclipse Thingweb™ offers multiple components that leverage the W3C WoT standards, which can be used for improving an existing solution or building a new one. Relevant components are listed below and more information can be found on Thingweb.io.

node-wot

node-wot is a Web of Things implementation in Node.js that allows interaction with IoT devices or to build IoT devices that support the WoT standards.

eclipse-thingweb/node-wot

Playground

Playground is a set of tools around WoT Thing Descriptions that allow to validate them or transform them to other API description formats.

eclipse-thingweb/playground


EXI and E-Mobility

The Efficient XML Interchange (EXI) format is a very compact representation for the Extensible Markup Language (XML).

ISO 15118 is the vehicle to grid (V2G) communication interface using the EXI format.

EXIficient

An open source implementation of the W3C Efficient XML Interchange (EXI) format specification.

EXIficient


OpenV2G

Project to support the ISO and IEC standardization process to specify the so called "Vehicle 2 Grid Communication Interface" (V2G CI) which became the ISO IEC 15118 specification by now.

OpenV2G

Want to join us?

Careers